Part Number: DS90UB983-Q1
Tool/software:
Hello! There is currently an application, as shown in the screenshot below. The SOC produces an image with a maximum resolution of 38400 * 2160, which needs to be divided into two images for display. One image is transmitted to 984 through FPD LINK IV and the other is transmitted to 948 through FPD LINK III. Please help confirm if this application is feasible, especially if there are two protocols, FPD LINK IV and FPD LINK III, on the same chip. Thank you.