Part Number: MAX3232
Other Parts Discussed in Thread: GD65232
Tool/software:
Hi Guys.
We are experiencing intermittent failures in the field with some of our units, occurring after random periods (from days to months). After investigation, we identified the RS232 MAX3232IPWR driver as a common point of failure. Specifically, the TX line (DOUT1) is shorting to GND, which causes the entire 3.3V line to short to GND. Removing the chip from the PCB resolves the issue.
The TX (DOUT1) is driving 2 to 3 RX receivers simultaneously which indicates that this could be the issue. But we've measured a few of these setups and does not see any overcurrent condition happening. We also have 100's of these configurations running in the field for more than a year.
Any ideas what could cause the chip to fail and how to fix the issue?
Thanks in advance.
Chip URL: