Part Number: TCAN1145-Q1
Tool/software:
Hi team,
Recently, we encountered a problem when debugging the wake-up function of TCAN1145 in our project. When the message with the same ID and data is sent through CAN, there will be a wake-up signal, but when it is sent using CAN FD format, there is no wake-up signal. However, our network management is in CAN FD format.
We found a description in the manual that only standard CAN wake-up is supported. I don’t know if it is related to the problem we encountered. Please confirm whether the TCAN1145 chip supports CAN FD for wake-up, and if so, which registers need to be configured.

Best regards!
Ethan