Part Number: SN65HVD72
Other Parts Discussed in Thread: THVD1406
Tool/software:
Hi,
We are going to be using the SN65HVD72 on an upcoming PCB as an interface for future communication with additional PCBs. At the moment, we do not have any PCBs to communicate with. Is there any way we can perform a test to ensure that the IC is working with our UART port and is ready for communication in the future?
In addition to this, would I be correct in understanding that, as this is a half-duplex device, I would need to toggle the IC when my microcontroller transmits and receives messages? Or can it be set up so that I do not need to toggle any GPIO and just focus on the UART data?