Part Number: AM26LS31M
Tool/software:
On page 4 of the datasheet, the pin numbers in Figure 4-2 do not match the pin numbers in Table 4-2 Pin Function. Which is correct please?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Frank,
Thanks for pointing this out.
On page 4 of the datasheet, the pin numbers in Figure 4-2 do not match the pin numbers in Table 4-2 Pin Function
I'll need to put in a change request for this to get it updated. (This isn't a fast process and requires approvals from multiple people on a committee so it will take some time).
Which is correct please?
The figure/image is the correct one. The table looks like a copy paste of the other packages.
Also, there is no pad drawing for the LCCC package at the end of the datasheet. There is only a picture of an LCCC package
On our internal system, I was able to find 2 drawings but I don't know which one of these is correct. It looks like the difference is related to the top pad sizing , shape of pin 1, and the thickness of the top side.....
The recommended soldermask and stencils look the same though.
I've attached the one I think should be the correct one based on the picture in the datasheet.
For reference, this is the other one in the system.
-Bobby