Tool/software:
Hi Expert,
This is Shenzhen FAE Evan. My customer use TCA9517A as a buffer between system SOC I2C port and external HDMI I2C port as shown in the schematic below. And A side is connected to external HDMI port, B side is connected to internal system SOC I2C. The issue is that, one test item of HDMI certification is the port input capacitance(should be below 50pF@100kHz I2C signal). The input capacitance Ci can be found in datasheet 13pF, I need to know how this parameter is measured, when IC is enable or not? When IC is enable, will the circuit after SCLB and SDAB have an influence on the total input capacitance at HDMI1_SCL_IN and HDMI1_SDA_IN? If TCA9517A can not remove the after-stage circuit capacitance influence, what device is recommended here?