Part Number: SN65HVD230
Other Parts Discussed in Thread: ESD2CAN24-Q1, ESD2CAN36-Q1
Tool/software:
Using the SN65HVD230DR CAN transceiver with an MCP2515 CAN controller.
This is successful past circuit being used in a new application.
Running both chips from 3.3V from a RasPi4 compute module.
Wiring and connections are all verified correct.
With CAN bus open circuit, didn't find any problems after numerous power cycles (while testing other circuits on the board).
The CAN bus is only used for point-to-point communications with a CAN motor controller (CubeMars AK Series).
After making the CAN bus connection, our CAN transceiver chip immediately failed on first power-up, and also seems to have taken out the CAN motor controller.
Our chip now measures 2.5 ohms between the Vcc and ground pins.
Replacing with new chip on our board, it seems okay but haven't tried connecting to our remaining good CAN motor controller yet (gun shy).
Could the fact that the RasPi4 3.3V output is delayed about 150 ms have anything to do with the failure?
The motor and controller are powered up coincident with the RasPi, but our CAN circuit only powers up 150 ms later.
Thanks,
Mark