Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRS3232E-Q1: short to Battery

Part Number: TRS3232E-Q1
Other Parts Discussed in Thread: SN65HVD1780-Q1

Tool/software:

As described in the specification, the maximum withstand voltage of the Dout pin is ±13.2V, but the short circuit to power supply test of the car requires a short circuit to 14V. Will this cause damage to the chip? If a TVS with a clamping voltage below 13.2V is selected, the TVS may be directly burned out when short-circuited to the power supply. So how should I choose a protective device?