Part Number: DS90UR124
Other Parts Discussed in Thread: DS90UR241, DS90UR241-Q1,
Tool/software:
I am trying to implement the DS90UR241/DS90UR124 Serializer/Deserializer FPD Link II chipset. In the datasheet for these two devices, the 24 LVCMOS parallel output pins for the deserializer are listed as Rout0 through Rout23. However, these chips seem to only be capable of RGB666 18 bit color, and not 24 bit color. I would assume that 18 output lines are for color, one line is for HSync, one line is for VSync,
The datasheet does not seem to specify which pins are for Red 0-5, Blue 0-5, and Green 0-5, along with HSync, VSync, and DE for sending to an LCD screen. Is there a specific pinout for these devices? If not, does the pin configuration of the deserializer output depend on the pin configuration of the serializer input? Since all the pins are digital data, it seems the actual lines are interchangeable and which pins are RGB666, HSync, VSync, and DE are dependent on the pcb design layout for the serializer.
Thanks in advance for any assistance.