Part Number: DS90UB983-Q1
Tool/software:
Hi,
We are now encountering some problems, need to debug dp dual-screen heterodyne, the serdes used is ti983 --> ti948, the original configuration is mst way, because the platform does not support mst, so we want to use sst+superframe way, through the reading of msa and other related registers to read to the front end of the dp signals are normal, but our own configuration by scripting But the configuration we generated through the script is not ideal, there is no display, you can play serdes-pattern, but this pattern is the same as the display, sst+superframe, if you need to use the Splitter mode, if so, we generated in accordance with the script configuration file does not have the setting of the splinter, please help to generate the sst+superframe configuration, please help to generate a sst+superframe configuration. superframe configuration, timing and block diagram as below, thanks!
#THW = Horizontal Total Pixels = AHW + HBP + HFP + HSW -------- 2052
# TVW = Vertical Total Lines = AVW + VBP + VFP + VSW -------- 761
# AHW = Hoizontal Active Pixels -------- 1920
# AVW = Vertical Active Lines -------- 720
# HBP = Horizontal Back Porch Pixels -------- 32
# VBP = Vertical Back Porch Pixels -------- 6
# HFP = Horizontal Back Porch Pixels -------- 72
# VFP = Vertical Back Porch Pixels -------- 30
# HSW = Horizontal Sync Width Pixels -------- 28
# VSW = Vertical Sync Width Lines -------- 5
# HSP = Horizontal Sync Polarity: 0 = Positive, 1 = Negative -------- 1
# VSP = Vertical Sync Polarity: 0 = Positive, 1 = Negative -------- 1
# PCLK = Pixel Clock Rate in MHz -------- 93.70MHz
# Bits_per_pixel = 18, 24, or 30 (30bpp only available for FPD IV) ------ 24