Part Number: DSLVDS1047
Other Parts Discussed in Thread: DSLVDS1048
Tool/software:
Hello guys,
One of my customers uses DS90LV031ATM/NOPB and DS90LV032ATM/NOPB for their current products.
They are considering replacing DS90LV031ATM/NOPB with DSLVDS1047.
At this moment, they have the following questions.
Could you please give me your reply?
Q1.
DSLVDS1047 datasheet says on page 13 that "Open Input Pins. The DSLVDS1048 is a quad receiver device,
and if an application requires only 1, 2, or 3 receivers, the unused channel(s) inputs must be left OPEN.
Do not tie unused receiver inputs to ground or any other voltages."
I think DSLVDS1048 in this sentence is incorrect and the correct sentence is that the DSLVDS1047 is a quad receiver device...
Is my thought correct?
Q2.
This is just confirming. If DSLVDS1047 has no used pin at DIN1~4, must the pin be left OPEN?
Q3.
Is there any problem at DSLVDS1047 and DS90LV032ATM/NOPB combination?
Your reply would be much appreciated.
Best regards,
Kazuya.