Part Number: TL16C750
Other Parts Discussed in Thread: TL16C550C,
Tool/software:
Dear Specialists,
My customer is evaluating TL16C750 and TL16C550C. They has aquestion.
I would be grateful if you could advise.
---
Are there any differences in the software between the TL16C750 and TL16C550C?
When I set up the same software, the frequency output from the BAUDOUT terminal
was 460kHz for the TL16C750 , on the other hand 450Hz for the TL16C550C, which is 1/1,000.
The TL16C750 is a pin compatible device with the TL16C550B/C, and the explanations of the BAUDOUT terminal, Baud Generator Timing Waveform, internal block diagram, DIVISOR and Baud Rates are all exactly the same.
Could you please advise what the differences and how can I make them the same?
---
I appreciate your great help in advance.
Best regards,
Shinichi