Part Number: THVD1400V
Other Parts Discussed in Thread: AMC1400, THVD1400
Tool/software:
Hello Support,
I have an IC which I have not identified.
Is it THVD1400V?
You can find related picture below.
Please advise
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ti.com/packaging/en/docs/partlookup.tsp?partmarking=1400 says that "1400" is either THVD1400 or AMC1400, and this is certainly not the AMC's extra-wide SOIC package. The THVD1400V would be in a SON package.
Thank you very much. I think it is THVD1400. It is very close to RS485 connector. I already checked parts lookup and found that THVD1400 has only WSON package. I confused and wrote here. Do you have any info that THVD1400 has SOIC package?
The THVD1400 is available in SOIC and SOT-5X3 packages. (The LCSC photo looks OK.) The THVD1400V is available in the VSON package, but its marking would be "1400V".