Other Parts Discussed in Thread: TPS629206,
Tool/software:
Hi,
We are implementing a USB 3.2 GEN2x1 mux/re-driver with TUSB1142. After reading the datasheet, the following is not quite clear to me:
5.3 Recommended Operating Conditions: "V(PSN) Supply Noise on VCC pins (less than 4MHz) <50mVpp"
- Does that mean 50mVpp are allowed in the frequency range below 4MHz? If yes, which ripple voltage is allowed above 4MHz? Do you have any PSRR values for TUSB1142?
(The goal is to decide if a TPS629206 based dc/dc-converter is practical or if we need a LDO (not favoured).)
The datasheet says on the first page "Advanced USB power management – Active: 550mW (typical)" and in chapter "5.5 Power Supply Characteristics" PACTIVE-USB-1Port = 275 mW (typical)
- In which case does TUSB1142 draw 550mW (typical)? (I assume that driver and receiver for the not selected lane will be switched off)
- What is the maximum supply current? (to design the power supply)
8.2.1 Design Requirements, Figure 8-1 / Table 8-1
- In which cases are the optional AC-coupling capacitors recommended?
(I have seen 7268.USB 3.1 ECN Rx AC Coupling Capacitor Option.pdf in another forum post but that does not a clue why to add AC-coupling capacitors or why better not)
Thanks, Michael