Part Number: TCAL9539-Q1
Other Parts Discussed in Thread: TCAL9539,
Tool/software:
hi,
there are no VIL and VIL in TCAL9539-Q1. What are them?
below is VIH/VIL in TCAL9539 for reference.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAL9539-Q1
Other Parts Discussed in Thread: TCAL9539,
Tool/software:
hi,
there are no VIL and VIL in TCAL9539-Q1. What are them?
below is VIH/VIL in TCAL9539 for reference.

Hi Ken,
The TCAL9539-Q1 was derived from the TCAL9539. As Clemens has suggested, the values should be the same. We can also refer to the timing diagrams for more information on the level.

Conditions are still set at 70% of VCC = VIH, and 30% of VCC = VIL.
Regards,
Tyler