Part Number: TUSB212EVM
Tool/software:
I used the HS detection circuit on transistor Q1 .

When the VREG signal 1.8V appears, the LED does not light up. The LED itself receives a voltage of 1.4V. At the same time, the LED should have a voltage of at least 2.0V. If you swap resistor R2 and LED D1, the indication starts to work normally.
Is this an error in the circuit?