Part Number: TCA6424A
Other Parts Discussed in Thread: TCA6424
Tool/software:
Hello,
I am using the TCA6424A in the design.all ports are configured as inputs and the host is successfully able to detect the state change on each port. However, the INT pin stays high. it never asserts low even on pin state changes. I have two boards with 2 different versions of the IC. One chip is marked "L6524" which doesnt assert the INT and the other is marked "PH424A" which asserts the INT pin everytime. what is the difference in the markings and how can I fix it on t he IC on which the INT doesnt work.