Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: Compliance Test

Part Number: DP83867IS

Tool/software:

Hi All,
 

I have a question about the Ethernet Compliance Test for the DP83867ISRGZ.

I am referring to the following application note:
https://www.ti.com/lit/an/snla239c/snla239c.pdf 

(1) Regarding 2.3.8 Return Loss, do both the Transmitter and Receiver need to be set to Test Mode 5?

(2) The actual test needs to be performed with and without the Twisted Pair Model, but there is no mention of the Twisted Pair Model in 2.4.1 Link Pulse.

Which Twisted Pair Model should I set it to? Do I need to perform both?

Best Regards,
Ishiwata