Part Number: DS160PR810
Tool/software:
Hello:
I have some questions here, please help confirm:
1. The manual says that it can support PCIE4.0 channel loss up to 42dB, and the maximum PCIE4.0 protocol channel loss is 28dB. Can it be understood that the additional extended routing loss needs to be controlled within 14dB?
2. Our application scenario is from the chip to the gold finger of the board. The link is very long and needs to be added with a Redriver. The entire link is as shown below. The PCIE4.0 CEM protocol requires that the board routing loss is within 5dB. We want to extend it to nearly 19dB. Can this Redriver support it? Are there any other questions?
3. The PCIE4.0 CEM protocol requires that the board routing delay Delay cannot exceed 750ps, as shown in the figure below. Our link is long (which is why we need to add a Redriver), plus the delay of the Redriver, it will definitely exceed this requirement. Will there be any problems? Does your company have experience in dealing with similar problems?
4. The manual states that the latency difference (skew) between different lanes of the same redriver is +/-20ps. What is the latency difference between lanes of different redrivers? We are using x16 PCIE and need to control the latency between two groups of x8 to meet the specification requirements.