Part Number: TCA9617A
Other Parts Discussed in Thread: TXU0101
Tool/software:
Hi guys,
is there anything to use to shift the level (e.g. 5V to 1.8V) for a MIPI RFFE interface which is bidirectional? Speed doesnt matter.
Cheers,
Marks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TCA9617A (or any other I²C level shifter) can be used for any bidirectional open-drain signals. As far as I can see, SCLK and SDATA have pull-downs at the master, so they are not compatible with open-drain signals.
The SCLK signal is unidirectional, so you could use the TXU0101. But I think that there is not any integrated translator that can handle SDATA.
Alright - I was afraid that there is nothing what makes it more comfortable. So just grad an IC (like the SN74LVC8T245QPWRQ1) where I manually change the direction of that levelshifter for SDATA...