Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1142: TUSB1142 not working on device-side

Part Number: TUSB1142
Other Parts Discussed in Thread: TUSB1004, TUSB1104

Tool/software:

Hi,

We are using the TUSB1142 SS mux on the device side, not host-side, and are not getting any SS communication. It is fully I2C controlled and only the EN and SLP_SO# signals are connected (both driven high with MCU). At this point I am manually selecting the mux orientation (FLIP_SEL in General_1 register). I am leaving all settings at their default values, except for controlling FLIP_SEL and CTLSEL (set to 0x01) in General_1. Monitoring both USB1_STATUS and USB2_STATUS registers they never show anything other than 0x01 (disconnected state). I have a few questions to hopefully help with debugging the issue:

  1. The datasheet mentions that the TUSB1142's SSTx and SSRx signals can be connected to either a host or a device, but all diagrams, examples, and pin descriptions are only for use with a host. Can you confirm that SSRx and SSTx connected to a device is a valid use case?
  2. Are the initialization and control steps outlined above correct and sufficient to get SS communication working?
  3.  Are USB1_STATUS and USB2_STATUS referring to the CRxX/CTxX interfaces on the mux?
  4. When SSRx/SSTx are open (i.e. no device connected) and a host is attached to CRxX/CTxX via a cable, should either USB1_STATUS or USB2_STATUS indicate anything other than 0x01?
  5. Are there any other registers that might help debugging this? I see there are quite a few RESERVED bits and a lot of "holes" in the I2C register memory map, so I'm wondering if there's anything else that's not documented in the datasheet.
  • Hi,

    1. Yes, you can use the 1142 on the device side of the type-C connection.

    2. You may need to change the EQ settings on our device to get SS communication working. If EQ is too low or too high, the signal can be unrecognizable on the host or device end.

    • Additionally, if VIO_SEL is floating make sure the I2C voltage is 3.3V

    3. Yes, USB1_STATUS is for CTX1/RX1 and USB2_STATUS is for CTX2/RX2

    4. Our device needs to see connections on both sides to exit disconnect mode. You need a host and a device connected.

    5. I have a few questions to get a better idea of the issue:

    • Are you connecting both a host and device when you test the 1142? The 1142 needs to see terminations on the TX pins before it transitions to the polling state.
    • How much power does our device draw? In the disconnect state we expect around 1.5mW. If the device is drawing more power, it should be entering active mode

    • Do you see any signal passing through the 1142 between the host and device?
    • Can you share the schematic of the 1142 and the routing to your USB connector? I'd like to see if there's an issue with the implementation. You can share this here or privately by requesting friendship on E2E and using the direct messaging feature.

    Best,

    Shane

  • Hi Shane,

    Thanks for your reply and the confirmation that how we want to use this part is correct. I did find a few things that were wrong on our side and have been able to get a SS connection at last. But there are still a few quirks to work through. 

    We had the SSRx and SSTx signals swapped. We have a special application with cables on both sides. The device side is a captive cable where orientation is fixed, but the cable still flips the Rx/Tx signals just like a regular cable. Since the TUSB1142 essentially performs the "cable flip" by SSRx being a transmitter and SSTx being a receiver we essentially had a double-flip, which is of course wrong. I simply misread the datasheet. The diagram in section 7.2 helped clear up any confusion.

    Although things are working now I was wondering if you could explain a few I2C register bits for me. I have the FLIP bit set, which switches the mux to CRx2 and CTx2 (pins 36/37 and 39/40), but the connection seems to be indicated in USB1_STATUS via bit U0 (0x04) and not in USB2_STATUS as I expected. Are they flipped?

    Also, when the SS connection was established, the USB2_STATUS register read 0x41. This is still disconnected state, but bit 6 was now set and the datasheet defines it as RESERVED. Do you know what this bit indicates?

  • Hi,

    I'll need to confirm whether the USB_STATUS registers are flipped or not. I have a question about the behavior to help narrow this down:

    • Does the USB2_STATUS or USB1_STATUS U0 bit get set when you keep FLIP at 0 (normal orientation)? Note you may need to flip the type-C cable as well for the connection to go through.

    Reserved registers are for TI testing purposes and are not intended for customer use. Unfortunately I cannot share what that bit indicates.

    Best,

    Shane

  • Ah, good question. Here are the I2C register results for both cases:

    No Flip:

    GENERAL_1 : 0x11

    USB1_STATUS: 0x44

    USB2_STATUS: 0x01

    Flipped cable:

    GENERAL_1: 0x15

    USB1_STATUS: 0x04

    USB2_STATUS: 0x41

    This doesn't really make sense. The U0 bit is set only in USB1_STATUS while USB2_STATUS always indicates disconnected state. The only real difference is the reserved bit 6 that follows the flip. I do see that the AEQ1_STATUS register has some bits set when the cable is not flipped and when it is flipped then the same bits are set in AEQ2_STATUS, so that follows the orientation. 

    By the way, I have the mux working as expected in both orientation, so I can resolve the issue, but I'm really curious about the USBx_STATUS register behavior. It would be really nice if we could use these two registers for debugging purposes to see which one has the active connection.

  • Hi,

    I checked internally and apparently both CTX1/RX1 and CTX2/RX2 will use the same state machine in the 1142. I apologize for the confusion here.

    This means USB1_STATUS shows the status of the 1142 state machine in both orientations. USB2_STATUS should be ignored. I believe USB2_STATUS was included from similar parts (TUSB1004/TUSB1104) that use two separate state machines. Since the 1142 only has one through-connection, there is only one state machine necessary.

    It would be really nice if we could use these two registers for debugging purposes to see which one has the active connection.

    Since you write the FLIP_SEL bit, you could use that to determine the active connection lane.

    Best,

    Shane