This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9517A: About TCA9517A

Part Number: TCA9517A
Other Parts Discussed in Thread: TCA9517

Tool/software:

◆Question

 This device (TCA9517A) and the TCA9517 have the same terminals.

 Are the internal specifications the same?

 Is the TCA9517A a suitable replacement for the TCA9517?

Best regards

  • The datasheet says:

    The TCA9517A offers a higher contention level threshold, VILC, than the TCA9517, which allows connections to slaves which have weaker pulldown ability.

  • ◆Additional questions

    >The TCA9517A offers a higher contention level threshold, VILC, than the TCA9517, which allows connections to slaves which have weaker pulldown ability.

    ⇒ In other words, can a larger pull-up resistor be connected to the TCA9517A compared to the TCA9517?

    Also, other than VILC, are there any other specification differences compared to TCA9517?

    Best regards

  • Both TCA9517 and TCA9517A support many different pull-up resistors. The question is how low the worst-case VOL of your other I²C devices is.

    As far as I can see, there are no other differences.

  • User6448843,

    >The TCA9517A offers a higher contention level threshold, VILC, than the TCA9517, which allows connections to slaves which have weaker pulldown ability.

    ⇒ In other words, can a larger pull-up resistor be connected to the TCA9517A compared to the TCA9517?

    "larger pull-up" as in stronger pull-up yes. Stronger means smaller resistance value which would push the VOL higher. VILC = 0.45V allows for more margin here. 

    Also, other than VILC, are there any other specification differences compared to TCA9517?

    VILC is the only change. 

    Regards,

    Tyler