Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN330G: TCAN330G

Part Number: TCAN330G
Other Parts Discussed in Thread: TCAN332G, TCAN330, TCAN337G, TCAN334G

Tool/software:

We are using TCAN330G is compatible with the ISO 11898 High Speed CAN. 

TCAN330's datasheet tells that 'Pending the release of the updated version of ISO 11898-2 including CAN FD, additional timing parameters defining loop delay symmetry are specified for the TCAN330G, TCAN332G, TCAN334G and TCAN337G devices. The devices include many protection features'

Can u please update us on release?

Or Please confirm can i use TCAN330G for CAN FD?

Is it CAN FD compatible?