Part Number: THVD1429
Other Parts Discussed in Thread: THVD1450, THVD1420, THVD1400, , SN65HVD23
Tool/software:
Hello,
we use two RS-485 transceivers to transmit data with max. 12.288 MHz (differential manchester encoding) over Cat 5e cable. One transceiver is the transmitter, one is the receiver. The roles are randomly determined by connecting two devices for the first time. We initially aimed for 50 m cable length. During development we tried different transceivers in the following order:
- THVD1450: Worked very well up to 50 m with margin. But we didn't pass the radiated EMC test. We assumed that the fast edges of this 50 Mbps transceiver played a role.
- THVD1400: We changed than to THVD1420 with only 12 Mpbs, being aware that our datarate is a already out of spec. But we passed EMC tests and the communication link worked. Later it turned out, that the link doesn't work reliably. With some devices it works over 50 m with others only over 10 m. Waveforms looked almost identical to THVD1450 so we assumed we're hitting the 12 Mpbs spec limit.
- THVD1429: We changed to the THVD1429 (20 Mbps) which works reliably over 30 m which at this point was OK for us. But strangely enough the waveforms looked really bad, see below.
The schematics are the same for the transmitting and receiving end.

Oscillograms from the THVD1420 over 50 m. Both differential signals on the left side, eye diagramm of the differential signal on the right side


THVD1429 with exactly the same test setup. It looks considerably worse, especially for the short bit times. The waveform looks not like the typical RC charging waveform. It's more like a straight at the beginning which indicates a current source. But I couldn't find any clues in the datasheet like a lower drive strenght that would explain this.


Any help is appreciated. Right now I'm not so sure the THVD1429 is the right part for the job or if there's something wrong with the schematic.
Best regards,
Florian