Part Number: TVS2700
Tool/software:
Hi all,
My customer was using the following configuration.
When I placed the TVS2700 between output and GND, I could confirm that it does not output even when TPS16416 is turned on.
Are there any conditions for using this TVS2700?
[For example]
・It is suitable only for large capacity power supply lines
・27V clamp voltage product is not suitable for 24V DC
If you know anything, please let me know.

Best Regards,
Ryusuke