Part Number: DS100BR111
Tool/software:
We plan on using the DS100BR111 configured as a 10G-KR repeater. We are getting into SI analysis of the design and have the following questions:
JITTER
- Typical deterministic jitter values (DJxx, see Nov2014 datasheet section 7.4 page 8) are rather high to insert the repeater reliably into a channel with pre-existing jitter, hence it is imperative we understand the repeater’s inherent jitter. Can TI provide additional jitter values (max values, other EQ settings, etc.)? Is there any other application info and/or measured data on repeater jitter? Assumption: no additional data is available beyond the datasheet and model.
- The part’s associated IBIS-AMI models (called from model DS100BR111.ibs rev 6.0 Sep2014) do not specify jitter parameters in either the Tx or Rx .ami files, nor does the model’s User Guide address jitter. As such, it seems we should add jitter, per datasheet values, using EDA tool constructs? Assumption: yes.
- The model’s User Guide quantifies “jitter” when comparing the AMI model’s performance to Cadence transistor simulation on pages 10 to 13. Can we assume these are simply values measured in the eye diagrams with no additional (datasheet-driven) jitter imposed in either simulation environment? Assumption: yes, the values in the Guide capture time variation that subtracts from eye width and calls this “jitter”.
- Simulating the above models into testloads, it appears that increasing EQ increases the device’s inherent jitter. Does TI agree with this observation? Assumption: yes.
- If our existing channel already has 0.30 UI jitter (channel only, no Tx or Rx), does TI agree that inserting the repeater will increase the end-to-end channel (repeater included) jitter linearly by the amount imposed by the repeater? Assumption: yes.
EQ
- The model and datasheet/User_Guide do not agree on either Tx or Rx EQ dB levels. Compare Rx min EQ and Tx max EQ levels. Which is correct? Assumption: datasheet.
- User Guide section 4’s VOD_Level Table (right column) says “De-emphasis value” which we believe to be peak-to-peak amplitude? Assumption: yes
TI can provide additional information on these questions, or simply confirm our assumptions are correct.
Thanks much,
Kevin