Part Number: DP83848K
Tool/software:
Hi exparts,
I have qustion about DP83848K link time. This is my first support for ethernet phy, so I hope your kindly support. If I need more information, please tell me.
Customer situation:
Two DP83848Ks are mounted on a single circuit pack. Two DP83848Ks were folded and connected for shipment testing. It took more than 30 seconds to establish the link. They want to know the cause.
*Two DP83848Ks are unreset at the same time.
*Two DP83848Ks are connected to each other with a straight-through cable. (TX-to-RX, RX-to-RX).
Q1. In the above configuration, each DP83848K will run Auto MDIX at the same time. Is it possible that by repeating TX and RX to each other, it will not be possible to connect or it will take a long time to connect?
Q2. Are there any reports or errata that this or other device is experiencing any of the above?
(This is an example of a device from another company, and there was errata information about the issue of not being able to connect and the connection taking a long time due to Auto-MDIX)
https://www.analog.com/media/en/technical-documentation/data-sheets/ADIN1200-silicon-anomaly.pdf
Q3. If Auto-MDIX cannot be connected to each other continuously, is it possible to grasp the situation by measuring the communication waveform, accessing registers, etc.?
Thank you for your support.
Regards,
Hiromu