Other Parts Discussed in Thread: TPD4E02B04
Tool/software:
We have some issues debugging tmds1204. Below is (HDMI Receptacle to TMDS 1204) and Layout(TOP layer/L2-GND)
MODE = “R” ; SCL/CFG = “0” ; SDA/CFG1 =”0”; AC_EN =”H” ; LINEAR_EN = “F”;
RX: DCGAIN = “F or 1” ; CTLMAP = “0 or F”; EQ =”F0 to 11”;
TX: TXPRE = “F”; TXSWG = “F”’
- TMDS-6G EQ=”F0 to 11” OK; SIGDET_OUT = 0V;
- FRL-8G/10G/12G Failed; SIGDET_OUT = 0~3.3V;
- Remove ESD (TPD4E02B04) , CTLMAP =”F”, FRL-8G/10G/12G Failed; SIGDET_OUT = 0~3.3V;
- Remove ESD (TPD4E02B04) , CTLMAP =”0”, FRL-8G OK/ FRL-10G/12G Failed; SIGDET_OUT = 0(8G);
- HDMI Receptacle is 2086581052 Molex;
- Layout Impedance control 100ohm±10%;
Is the problem with the input signal(ESD and 0 ohm-resistor Signal integrity)?
Are there any other parameters that can be adjusted?