Part Number: LMH1218
Other Parts Discussed in Thread: LMH1219, USB2ANY
Tool/software:
Hello,
We are using LMH1218 OUT0 interface (75 Ohms) to output 4K/12G-SDI video to an Eizo Monitor. The data interface is from Ultrascale FPGA with GTX rated at 12.5 Gbps.
However, we are able to output only 6G rates, and the 12G signal appears momentarily as "Signal error", and then permanently as "No Signal" on the monitor.
1) The initialization steps shown in the datasheet are followed, but there is no difference in operation with or without it.
2) The connector used is 75 Ohm HD-BNC series from Samtec, and the HDBNC-BNC cable used is only 1.5 meters.
2) The CDR always shows locked - can we assume that the FPGA interface is working OK?
3) If the above is true, it seems the only setting for the OUT0 driver is OUT0_VOD, without any de-emphasis settings. Is that correct?
Regards
Gaurav