This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB925Q-Q1: Can I use DS90UB925Q (FPD-Link3) → DS90UR124QVSX/NOPB (FPD-Link2)?

Part Number: DS90UB925Q-Q1
Other Parts Discussed in Thread: DS90UR124, DS90UR241

Tool/software:

Can I use DS90UB925Q (FPD-Link3) → DS90UR124QVSX/NOPB (FPD-Link2)?
If so, please tell me the settings required on the serializer and dserializer sides.

The DS90UR124 does not have I2C communication, so I think it can be used under the following conditions:
・DIN0-ROUT0 must be matched.
・The speed must be 43MHz or less, which is FPD-Link2.

Thank you very much.

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>> 
Kyoto Kanayama
Nippon Seiki Co., Ltd. NS Technical Center, Electronics Hardware
2-2-8 Higashi-Takami, Nagaoka, Niigata, 940-0006 Japan
>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>