Part Number: TCA9617B
Tool/software:
Hi Team
My customer wave form and datasheet wave form have 0.5V offset.

is it because SCH value wrong?

BRs
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9617B
Tool/software:
Hi Team
My customer wave form and datasheet wave form have 0.5V offset.

is it because SCH value wrong?

BRs
Brian
The pedestal would go only to near 0 V. The voltages marked in the red circle go below GND; this is probably ringing due to the high speed of the falling edge. Anything larger than −0.5 V is harmless. (If your oscilloscope probe uses a ground clip, then this ringing might be happening in the cable loop and not on the board; a ground spring would allow better measurements of high-frequency signals.)
Hi Clemens
below is feedback from customer
The R1385 and R1388 are adjusted to 510 ohm, but the undershoot is still near -0.5V.
In addition, we don’t want the value of these resistances to be too high. We hope the value will close to 0 ohm.
Under same schematic, the source from other vendors doesn’t generate the issue, so whether you can provide a solution for us to resolve
it.
falling of SCL

Falling of SDA

BRs
Brian
Hi Brian,
In addition to Clemens' feedback, I do not seem to see R1385 and R1388 in the provided schematic as well.
I presume they are series resistors and not pull-ups. If so, adjust closer to the transmission line (typically for 50 ohms). I.e. the output impedance of the device + series resistor should be closer to 50 ohms.
For example, output impedance of the device is 33 ohms with VOL of 0.1 V and IOL of 3 mA , R = VOL / IOL. Hence, series resistors of 17 ohms would suffice (50-33). Other vendor's output impedance can be closer to the transmission line used and may not have as much impedance mismatch to observe issue. You can confirm this if their rise / fall times are slower, thanks.
Best Regards,
Michael.