Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1145-Q1: spec vs TJA1145

Part Number: TCAN1145-Q1

Tool/software:

Hi expert,

my customer are evaluating the TCAN1145-Q1 to replace TJA1145, but now they don't find below spec in the datasheet, could you help provide the answer or tell me where can find below spec in the datasheet.

1 could TCAN1145 support SAE J2284-1 to SAE J2284-5

2 what is the value about the spec: ESD(MM)--(TJA1145 is -300V to 300V)

3 what is the value about the Spec: Vth(RX)dif--differential receiver threshold voltage (TJA1145 is 0.7V). 

4could TCAN1145 support the BUS dominant time-out function 

5 could you provide below test report:

  C&S IOP test report

IBEE EMC test report 

AEC-Q100 test report