Other Parts Discussed in Thread: PCF8574, TCA9554, TCA9554A, TCA9555, PCF8574A, PCA9554A, PCA9555, PCA9554, PCF8575
FAQ: Logic and Voltage Translation > IxC >> I2C IO Expander Schematic Checklist
|
IO Expander Checklist |
|
|
|
Check |
Status (good, bad, okay, ?) |
Comment |
|
Local Decoupling Capacitors |
|
Generally, a 0.1-uF capacitor is placed on VCC, as close to the device as possible |
|
Verify the schematic pinout matches the data sheet pinout |
|
|
|
Check that the pullup resistors are present on the SDA and SCL net within the schematic. |
|
|
|
Unused GPIO pins are biased to either VCC or GND via resistor |
|
Most of TI's IO expander portfolio do not include internal pull-up resistors on the p-port pins; the exceptions are PCF8575, PCF8574, PCF8574A, TCA9555|PCA9555, PCA9554|TCA9554, and TCA9554A|PCA9554A and therefore can be left floating. An alternative approach is after powering up the device, any unused p-port pins can be set as an output (does not matter if set high or low). |
|
Device address is unique on the bus unless using an I2C switch or I2C MUX to resolve conflicts |
|
|
|
If the device has a /RESET pin, bias the pin high (preferably with a pull-up resistor) after powering up. |
|
|
|
If the device has a /INT pin and the /INT pin is used, tie this pin to a pull-up resistor. |
|
|