Part Number: SN65DP141
Tool/software:
HI,
Two pcs of SN65DP141 are used in a my account with the connection architecture in the attach. would you like kindly help to recommend a initiation register configuration for SN65DP141?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DP141
Tool/software:
HI,
Two pcs of SN65DP141 are used in a my account with the connection architecture in the attach. would you like kindly help to recommend a initiation register configuration for SN65DP141?
Hey Ken,
I can provide a general template as follows.
IC1 script: 0x00 0011 0100 // I2C control, normal operation, all channel track channel 1, trace mode 0x01 0000 0000 //enable all channels 0x02 0xxx xxxx // channel 0 control 0x03 0000 0xxx // channel 0 enable stettings 0x05 0zzz zzzz // channel 1 control settings 0x06 0000 0z00 // channel 1 enable settings 0x08 0xxx xxxx // channel 2 control 0x09 0000 0xxx // channel 2 enable stettings 0x0B 0xxx xxxx // channel 3 control 0x0C 0000 0xxx // channel 3 enable stettings IC2 script: 0x00 0011 0000 // I2C control, normal operation, all channel track channel 1, cable mode 0x01 0000 0000 //enable all channels 0x02 0xxx xxxx // channel 0 control 0x03 0000 0xxx // channel 0 enable stettings 0x05 0zzz zzzz // channel 1 control settings 0x06 0000 0z00 // channel 1 enable settings 0x08 0xxx xxxx // channel 2 control 0x09 0000 0xxx // channel 2 enable stettings 0x0B 0xxx xxxx // channel 3 control 0x0C 0000 0xxx // channel 3 enable stettings
Please use the following table to tune the EQ to your system:

Vishesh
would you like to double check if the trace mode/cable mode corresponding to the EQ_mode pin and EQ_mode bit is the opposite?


Hey Ken,
These setting are for two different use cases. Pin 35 will determine the trace/ cable mode when the device is in pin-strap mode. This means that the I2C control is disabled.
In I2C mode pin 35 is the ADD2 pin which controls the address of the device. In I2C mode the register 0x00 controls the trace/ cable mode.
hi, Vishesh
Is there a document detailing the DC Gain and AC Gain parameters for DP141? DC gain and AC gain are best illustrated by comparing input and output waveforms of DP141.
Unfortunately, we do not have any illustrations comparing the DC and AC gain as the magnitude of the equalization will vary depending on trace length (insertion loss), and trace quality (return loss/ noise/ crosstalk).
We leave it up to the customer to properly tune the device. We have a reference schematic and layout available which may be helpful. The EQ is easily changeable, so the main focus of design when using the DPD141 is making sure the max EQ capabilities of the device meet the loss of the trace/ cable used.