Part Number: TVS0701
Other Parts Discussed in Thread: ESD401
Tool/software:
Dear Technical Support Team,
I'm looking for ESD protection for analog input/output.
Input/Output voltage is from 0V to 5V(DC level) and low leak current is required.
ESD resistance: over ±6kV
TVS0701(Target Application PLC I/O) is for TVS, however it seems to have enough spec for ESD(IEC 61000-4-2).
Leakage current is "at 0.25-nA Typical at 27°C, 200-nA Maximum at 85°C"

The leakage current for ESD401 is smaller like 10nA(max), 30pA(typ).
Is it possible to use ESD401 for analog input/output?
If you have any other recommended product, please let me know.
Best Regards,
ttd