Part Number: SN65LBC180
Tool/software:
We are using the IC SN65LBC180 in our design for RS485 communication and generally full duplex IC can be used as an half duplex IC by shorting the positive and the negative signals together.
during our testing of Half duplex we had the below observations.
->for transmission to occur the RE pin and DE pin both where set to low.
->for reception to occur the RE pin was set to low and the DE is set to high.
Kindly confirm if the setting of the DE and the RE for the transmission and reception is expected?