Part Number: TSB12LV26
Tool/software:
Looking at the technical documentation for this part (TSB12LV26), I see no information for the power consumption of the part. I need the typical / maximum power consumption for this part.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TSB12LV26
Tool/software:
Looking at the technical documentation for this part (TSB12LV26), I see no information for the power consumption of the part. I need the typical / maximum power consumption for this part.
Hi,
The TSB12LV26 is a very old part. I went back and searched its power number. Below is what I can find, these are measured power number.
| Vcc = 3.3 | ||||
| D State | CLKRUN# | Context | Icc (mA) | Power (mW) |
| D0 | Disabled | Initialized, LPS active, Cycle Master | 9 | 29.7 |
| D0 | Disabled | S200 Camera @ 320x240 30 FPS | 17 | 56.1 |
| D0 | Disabled | S200 Camera @ 320x240 15 FPS | 15 | 49.5 |
| D0 | Disabled | LPS inactive, Uninitialized | 7 | 23.1 |
| D3 | Disabled | LPS inactive, Uninitialized | 4 | 13.2 |
With VCC at 3.3V, these look to be the typical power consumption number. I do not have the max power consumption number. I also no longer have a setup which I can measure it.
Thanks
David