Part Number: DP83TG720R-Q1
Tool/software:
question:The 0x63c register has a value of 0xDE, but the rx_ctrl pin is not raised and the rxd data line does not emit data; Shouldn't rx send data when it receives it ?What causes this problem?
Some register values are as follows:
Register 045D is: D180
Register 1834 is: 8001
Register 0542 is: 0022
Register 0543 is: 0024
Register 0544 is: 2320
Register 0545 is: 0029
Register 0546 is: 0020
Register 0547 is: 0400
Register 0548 is: 0001
Register 3901 is: 0000
Register 3902 is: 0500
Register 3903 is: 0000
Register 3904 is: 0003
The schematic diagram is as follows: