Part Number: SN65HVDA540
Other Parts Discussed in Thread: RM46L852, TCAN4550-Q1, RM57L843
Tool/software:
Hello,
I need to communicate the RM46L852 MCU with 4 independent 250kbps CAN networks. Said MCU has 3 independent CAN controllers, of which one is currently being used in my application. How could I use one of the CAN controllers currently available on my RM46 MCU to communicate with 4 different CAN networks? Do you provide a specific IC for that purpose, something like a CAN demultiplexer?
Another possibility I was thinking of is to use an extra MCU (simpler than the RM46) with 5 CAN controllers, acting as a sort of CAN demultiplexer. Having 5 CAN controllers would be to use one of them as a communication method with the main MCU at 1Mbps Could you tell me if you have an MCU with >5 can controller?
Thank you very much.