Part Number: TCAN1043A-Q1
Tool/software:
Hi support:
According to the TCAN1043A-Q1 State Machine, during the shutdown process, if there detect a wake-up source when transceiver stays in the state of GO-TO-Sleep,
then the transceiver enter the standby Mode:

so INH pin always equal to high and SBC can not detect rising edge which will lead SBC to the standy state(SBC state).
Then Vcc and Vio fall below the UVcc and UVio, the transceiver will wait over tuv to lead transceiver to the Sleep mode .

1.Is my explanation correct?
2.Is this the only way to detect rising edge of INH pin?
3.if happen this case, there will be tuv(100-350 ms) delay during the initialization process?
4.How to avoid this case? Because There are requirements for initialization time,if happen this case, the initialization time will increase 100-350 ms,it can not met requirement.