Part Number: LM5013
Tool/software:
hi team,
my customer wants to use lm5013 to run at Vin:36V, Vo:12V with the constant current 3A. The SCH and PCB is as below.
The solution can only run to 2.7A and the temp of the chip will rise to 110℃.When they run the 3A output current ,the system can only wok well lasting 30min. the system will go wrong after 30mins.
Do u have any advise on the improvement of the thermal or do we have some thermal simulation to help customer lay out? thanks!