Part Number: TS3USB221E
Other Parts Discussed in Thread: TS3USB221, , TS3USB221A
Tool/software:
Do you have availability difference between TS3USB221 and TS3USB221E?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TS3USB221E
Other Parts Discussed in Thread: TS3USB221, , TS3USB221A
Tool/software:
Do you have availability difference between TS3USB221 and TS3USB221E?
Hi,
Please see the table below of the differences. The main differences are in the bandwidth performance and the enhanced ESD protection which are the main technical trade offs between these devices.
| Part Number | Mux Configuration | Switch Configuration | Channel (s) | Bandwidth typ (MHz) | Digital input capacitance typ (pF) |
COM On Capacitance @ 1Mhz typ (pF) |
COM off capacitance @ 1MHz typ (pF) |
NO/NC on capacitance @ 1MHz typ (pF) |
NO/NC off capacitance @ 1MHz typ (pF) |
ESD (V) HBM | ESD (V) CDM |
| TS3USB221 | 1:2 | SPDT | 2 | 1100 | 1 | 5 | 3 | 5 | 3 | 2000 | - |
| TS3USB221E | 1:2 | SPDT | 2 | 1000 | 1.5 | 6 | 3.5 | 6 | 3.5 | 12000 | 7000 |
| TS3USB221A | 1:2 | SPDT | 2 | 900 | 3.5 | 6 | 3.5 | 6 | 3.5 | 7000 | 1000 |
Thanks
David