Part Number: DS25CP114
Tool/software:
Hello teams
I appreciate your continuous support.
I would like to ask a question about the following TI device.
Target device: DS25CP114TSQE/NOPB
The device of five DS25CP114TSQE/NOPB are mounted on a board that is an our ASIC evaluation board.
Three of them failed (probably at the same time) during operation, causing a short circuit between the power supply (VDD) and GND within the device.
I would like to investigate the cause of this problem, so I would like to ask/consult about the following three points.
①What do you think could be the cause of this device failing and causing a short circuit between the power supply and GND?
(It is possible that an irregular voltage was applied to this device due to a work error during the evaluation of the ASIC, but under what conditions could the power supply and GND be shorted?)
②Is it possible for the power supply and GND to be shorted due to failure due to aging of the device?
(The board in question was manufactured in 2018, so the device was manufactured before that.)
③Is it possible to analyze the failed device and determine the cause?
In particular, if it is deterioration due to aging, we are concerned that previously manufactured boards will suffer frequent failures in the future,
so we are asking this question to allay our concerns.
Thank you for your confirmation.
Best regards