Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ESD1LIN24-Q1: Process to request the IMDS for this component

Part Number: ESD1LIN24-Q1

Tool/software:

Hi We need your support to get IMDS data for all the products that we use in one of our design.

Currently, we are using the following TI products:

Mfg Part No. Description
ESD1LIN24DYFRQ1 TVS DIODES AUTO, 3-PF, 24-V, 30-KV ES
TPS7B8133QDRVRQ1 IC REG LIN 3.3V/5V 150MA 6WSON
DRV8899QWRGERQ1 Motor Controllers&Drivers Auto, 50-V&1.0-A
TPS1HC100BQPWPRQ1 100-mOhm 2.5-A Single CH Auto Smart High
TLIN1021ADRQ1 IC, PHY, LIN, Rev 2.2A, 20Kbps
INA180A3QDBVRQ1 IC CURR SENSE 1 CIRCUIT SOT23-5

These IMDS data need to be directed to our supplier account with the IMDS ID: 191503 (OSIE).