Part Number: TCA9801
Tool/software:
Dear Specialists,
My customer is considering TCA980x and has a question.
I would be grateful if you could advise.
---
It is assumed that the A side of the TCA980x will be connected to the slave board and pulled up on the slave board.
In this case, if the slave board is not connected, there is no pull-up resistor.
Will this cause the B side to become undefined?
Or, since the B side has a built-in pull-up, is the output determined to be H/L even if the A side is left open?
---
I appreciate your great help in advance.
Best regards,
Shinichi