Part Number: TUSB211A
Tool/software:
Hi TI team,
It is stated that the TUSB211A supports up to 5m cable length.
1. Does this translate directly to a 5m PCB trace length as well? If not, what is the supported trace length for the part?
2. If I have a 13 inch trace route for the USB2.0 (device to device connection), would I have to place the re-driver near the destination device? or can it be placed in the middle as well?
Regards,
Ken.