Part Number: DS90UB960-Q1
Tool/software:
Hi,
Does DS90UB960-Q1 support GMSL2/1 to CSI-2?
We want found replace part for ADI MAX96724/F/R. thanks!
max96724-3135058.pdf (mouser.tw)
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB960-Q1
Tool/software:
Hi,
Does DS90UB960-Q1 support GMSL2/1 to CSI-2?
We want found replace part for ADI MAX96724/F/R. thanks!
max96724-3135058.pdf (mouser.tw)
Jeff
HI Jeff,
The two technologies are not compatible.
Is there any reason an FPDlink SER cannot be used? I can provided compatible device to the ADI MAX96724/F/R.
Glenn
Hi Glenn,
I need check they most need GMSL2/1 to CSI-2 or not, does any compatible device to the ADI MAX96724/F/R can suggest to us?
Thanks!