Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS26LS31MQML: Output amplitude and common mode

Part Number: DS26LS31MQML
Other Parts Discussed in Thread: AM26C31M

Tool/software:

Hi There,

I cannot find a specification for the differential output voltage magnitude or common-mode output voltage. 

Am I missing this information or is it supposed to be calculated?

Thank you for your insight in advance.

As ever,

Tom

  • Yes; you can compute it from the VOH and VOL specifications, which imply at 100 Ω load. Typical values are shown in figure 10.

    (The AM26C31M specifies the values you want, but it's a CMOS device.)

  • Hi Tom,

    I believe that the parameters you are looking for are on page 3 of the datasheet, listed as VOH / VOL. For common-mode, the top of the table states "The following conditions apply, unless otherwise specified. +V = 5V, VCM = 0V".

    Best regards, Amy