Part Number: AM26LV31E
Tool/software:
I am using an AM26LV31E. Specifically AM26LV31EIRGYR.
I ground both G and G not. Based on the datasheet truth table, When pin 12 (G not) is driven low, pin 4(G) becomes a don't care. To me this configuration will keep the transmitter enabled at all times. This is my baseline assumption.
If my assumptions are correct, I am seeing odd behavior. My input to 1A (pin 1) is zero volts while my output on 1Y is high (Vcc level) and 1Z is low. Based on table 7-1 of the datasheet, output Y should follow the state of input A. Mine appears to be the complement 1Z output is 0 volts while 1Y is 3.3 volts when the input A = 0 volts.
Could any provide their thoughts as to why I may be seeing this behavior? Perhaps it is expected and I am misinterpreting the datasheet.