Part Number: TFP410
Tool/software:
I have come across TI's TF410 www.ti.com/.../TFP410 video driver chip and had a few questions I wanted to ask:
1. The datasheet mentions the chip's capability to generate a video stream of 1080p at 60Hz. However, there is no mention of higher refresh rates at lower resolutions. Specifically, we are wondering if it is possible to produce a video stream at 720p 120Hz using this chip.
2. Regarding the TFP410 chip's Lifecyle. the TI website says it is "Active" and all indications are that the chip will be in production and available for the next decade or so. Given that the chip is around 20 years old, does TI still recommend this part for new designs? Can we get more information on when the chip may be phased out?
Regards,
Mahdi